AXIS#.TEMP
Description
This parameter returns the measured temperature of the power module on the power board for the associated axis.
Examples
Usage
The parameter can be used to track board temperatures as they change during drive operation. There is at least one control board temperature measurement (e.g., DRV.TEMP) and one power board temperature measurement (e.g., AXIS1.TEMP).
Code
--> DRV.TEMP 52.367 (Control) [degC] --> AXIS1.TEMP 31.664 (Power1) [degC] --> AXIS2.TEMP 32.312 (Power2) [degC]
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-02-02-000 |
|
General Information
Type |
Read Only |
Units |
degC |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.TEMP |
5000h |
10h |
Signed32 |
- |
- |
Read only |
No |
AXIS2.TEMP |
5100h |
10h |
Signed32 |
- |
- |
Read only |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
5026 |
1 |
5026 (0x13a2) |
AXIS1.TEMP |
Signed32 |
Read Only |
Yes |
70562 |
2 |
5026 (0x13a2) |
AXIS2.TEMP |
Signed32 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.TEMP |
5026 |
Float |
Read Only |
- |